Solution


Boat Hoist

A customer needs a boat hoist system in order to lift boats out of water for maintenance purposes. They would like a wireless solution in order to monitor the forces being applied through the hoist system.


BoatHoistGraphicColor 1

Summary

  • Customer Need / Challenge

    A customer needs a boat hoist system in order to lift boats out of water for maintenance purposes. They would like a wireless solution in order to monitor the forces being applied through the hoist system.

  • Interface Solution

    Interface suggests using multiple WTSSHK-B Wireless Crosby™ Bow Load Shackles at the pick up points of the hoist mechanism. Data results of the individual loading points and total weight can be transmitted wirelessly to the WTS-BS-4 Industrial USB Base Station when connected to a PC or laptop with supplied Log100 software.

  • Results

    Interface’s wireless system and solution successfully measured the weight of the boat and ensured it would be safely lifted out of the water.

Materials


  • WTSSHK-B Wireless Crosby™ Bow Load Shackles
  • WTS-BS-4 Industrial USB Base Station with supplied Log100 software
  • WTS-HK-S Next-Generation Wireless Handheld
  • Customer PC or Laptop

How it Works


  1. Multiple WTSSHK-B Wireless Crosby™ Bow Load Shackles are installed to the boat hoist mechanism.
  2. The boat is lifted out of the water, and the force measurements are wirelessly transmitted to the WTS-BS-4 Industrial USB Base Station. The customer can measure the individual loading points and total weight.
  3. When connected to a PC or laptop, force data can be logged and graphed with Log100 supplied software. Loads can also be seen using the WTS-HK-S Next-Generation Wireless Handheld.

Download PDF